Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ProjectCurveBuilder.DirectionType |
ProjectCurveBuilder.DirectionType.ALONG_FACE_NORMAL
Represents Along Face Normal
|
static ProjectCurveBuilder.DirectionType |
ProjectCurveBuilder.DirectionType.ALONG_VECTOR
Represents Along Vector
|
static ProjectCurveBuilder.DirectionType |
ProjectCurveBuilder.DirectionType.ANGLE_TO_VECTOR
Represents Angle To Vector
|
static ProjectCurveBuilder.DirectionType |
ProjectCurveBuilder.DirectionType.TOWARD_LINE
Represents Towards Line
|
static ProjectCurveBuilder.DirectionType |
ProjectCurveBuilder.DirectionType.TOWARD_POINT
Represents Towards Point
|
Modifier and Type | Method and Description |
---|---|
ProjectCurveBuilder.DirectionType |
ProjectCurveBuilder.projectionDirectionMethod()
Returns the projection direction method
License requirements: None. |
static ProjectCurveBuilder.DirectionType |
ProjectCurveBuilder.DirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ProjectCurveBuilder.DirectionType |
ProjectCurveBuilder.DirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ProjectCurveBuilder.DirectionType[] |
ProjectCurveBuilder.DirectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ProjectCurveBuilder.setProjectionDirectionMethod(ProjectCurveBuilder.DirectionType directionMethod)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.