Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static PointSetBuilder.PatternLimitsType |
PointSetBuilder.PatternLimitsType.DIAGONAL_POINTS
The pattern limit is defined by two points.
|
static PointSetBuilder.PatternLimitsType |
PointSetBuilder.PatternLimitsType.PERCENTAGES
The pattern limit is defined by surface U and V values.
|
Modifier and Type | Method and Description |
---|---|
PointSetBuilder.PatternLimitsType |
PointSetBuilder.patternLimitsBy()
Returns the pattern limits definition setting.
|
static PointSetBuilder.PatternLimitsType |
PointSetBuilder.PatternLimitsType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PointSetBuilder.PatternLimitsType |
PointSetBuilder.PatternLimitsType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PointSetBuilder.PatternLimitsType[] |
PointSetBuilder.PatternLimitsType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PointSetBuilder.setPatternLimitsBy(PointSetBuilder.PatternLimitsType patternLimitsBy)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.