Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static PointSetBuilder.CurvePointsType |
PointSetBuilder.CurvePointsType.CHORDAL_TOLERANCE
Points will be created based on the chordal deviation of curve.
|
static PointSetBuilder.CurvePointsType |
PointSetBuilder.CurvePointsType.CURVE_PERCENTAGE
A point will be created at given curve percentage.
|
static PointSetBuilder.CurvePointsType |
PointSetBuilder.CurvePointsType.EQUAL_ARC_LENGTH
Points will be created at equal arc length along curve.
|
static PointSetBuilder.CurvePointsType |
PointSetBuilder.CurvePointsType.EQUAL_PARAMETERS
Points will be created at equal parameter spacing along curve.
|
static PointSetBuilder.CurvePointsType |
PointSetBuilder.CurvePointsType.GEOMETRIC_PROGRESSION
Points will be created with a geometric progression along curve.
|
static PointSetBuilder.CurvePointsType |
PointSetBuilder.CurvePointsType.INCREMENTAL_ARC_LENGTH
A point will be created at the arc length spacing input.
|
static PointSetBuilder.CurvePointsType |
PointSetBuilder.CurvePointsType.SPECIFIED_PROJECTION_POINTS
Points will be created at minimum distance to curve.
|
Modifier and Type | Method and Description |
---|---|
PointSetBuilder.CurvePointsType |
PointSetBuilder.curvePointsBy()
Returns the curve points definition setting.
|
static PointSetBuilder.CurvePointsType |
PointSetBuilder.CurvePointsType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PointSetBuilder.CurvePointsType |
PointSetBuilder.CurvePointsType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PointSetBuilder.CurvePointsType[] |
PointSetBuilder.CurvePointsType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PointSetBuilder.setCurvePointsBy(PointSetBuilder.CurvePointsType curvePointsBy)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.