Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static PatternFaceBuilder.PatternTypes |
PatternFaceBuilder.PatternTypes.CIRCULAR
This stands for circular pattern type.
|
static PatternFaceBuilder.PatternTypes |
PatternFaceBuilder.PatternTypes.MIRROR
This stands for mirror pattern type.
|
static PatternFaceBuilder.PatternTypes |
PatternFaceBuilder.PatternTypes.RECTANGULAR
This stands for rectangular pattern type.
|
Modifier and Type | Method and Description |
---|---|
PatternFaceBuilder.PatternTypes |
PatternFaceBuilder.type()
Returns the pattern face type, don't use it until nx502
License requirements: None. |
static PatternFaceBuilder.PatternTypes |
PatternFaceBuilder.PatternTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PatternFaceBuilder.PatternTypes |
PatternFaceBuilder.PatternTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PatternFaceBuilder.PatternTypes[] |
PatternFaceBuilder.PatternTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PatternFaceBuilder.setType(PatternFaceBuilder.PatternTypes patternType)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.