Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static PatchOpeningsBuilder.OutputTypes |
PatchOpeningsBuilder.OutputTypes.MULTIPLE_FEATURES
Output one feature for each patch sheet body
|
static PatchOpeningsBuilder.OutputTypes |
PatchOpeningsBuilder.OutputTypes.SEW
Sew patch sheet bodies into target sheet body
|
static PatchOpeningsBuilder.OutputTypes |
PatchOpeningsBuilder.OutputTypes.SINGLE_FEATURE
Output one feature containing all patch sheet bodies
|
Modifier and Type | Method and Description |
---|---|
PatchOpeningsBuilder.OutputTypes |
PatchOpeningsBuilder.output()
Returns the type of output desired - one feature, multiple features, sewn.
|
static PatchOpeningsBuilder.OutputTypes |
PatchOpeningsBuilder.OutputTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PatchOpeningsBuilder.OutputTypes |
PatchOpeningsBuilder.OutputTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PatchOpeningsBuilder.OutputTypes[] |
PatchOpeningsBuilder.OutputTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PatchOpeningsBuilder.setOutput(PatchOpeningsBuilder.OutputTypes type)
License requirements: nx_freeform_2 ("advanced freeform modeling") OR die_engineering ("DIE ENGINEERING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.