Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static PasteFaceBuilder.PasteOptionType |
PasteFaceBuilder.PasteOptionType.ADD
each tool body will add to the target body.
|
static PasteFaceBuilder.PasteOptionType |
PasteFaceBuilder.PasteOptionType.AUTOMATIC
determined automatically from the 'add' or 'subtract' attributes on each tool body.
|
static PasteFaceBuilder.PasteOptionType |
PasteFaceBuilder.PasteOptionType.SUBTRACT
each tool body will subtract from the target body.
|
Modifier and Type | Method and Description |
---|---|
PasteFaceBuilder.PasteOptionType |
PasteFaceBuilder.pasteOption()
Returns the paste option defines whether the tool body is additive or subtractive.
|
static PasteFaceBuilder.PasteOptionType |
PasteFaceBuilder.PasteOptionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PasteFaceBuilder.PasteOptionType |
PasteFaceBuilder.PasteOptionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PasteFaceBuilder.PasteOptionType[] |
PasteFaceBuilder.PasteOptionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PasteFaceBuilder.setPasteOption(PasteFaceBuilder.PasteOptionType pasteOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.