Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static PartModule.PartLoadOption |
PartModule.PartLoadOption.DONT_ALLOW_SAVE
Sets the loaded part as read only.
|
static PartModule.PartLoadOption |
PartModule.PartLoadOption.LOAD_INTERPART
If this option is set, First it will check part is modified or not, then loads interpart of Part Module otherwise reload the own part of Part Module
|
Modifier and Type | Method and Description |
---|---|
static PartModule.PartLoadOption |
PartModule.PartLoadOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartModule.PartLoadOption |
PartModule.PartLoadOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartModule.PartLoadOption[] |
PartModule.PartLoadOption.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.