Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static PartGeometryCopyBuilder.Type |
PartGeometryCopyBuilder.Type.AUTOMATIC
An option to select point, datum, sketch, body, and curve feature
|
static PartGeometryCopyBuilder.Type |
PartGeometryCopyBuilder.Type.BODY_COLLECTOR
An option to select bodies via body selection intent
|
static PartGeometryCopyBuilder.Type |
PartGeometryCopyBuilder.Type.BODY_OBJECT
An option to select body, body-based feature, and body group
|
static PartGeometryCopyBuilder.Type |
PartGeometryCopyBuilder.Type.COMPOSITE_CURVE
An option to composite a curve via curve selection intent
|
static PartGeometryCopyBuilder.Type |
PartGeometryCopyBuilder.Type.COMPOSITE_FACE
An option to composite a body via face selection intent
|
static PartGeometryCopyBuilder.Type |
PartGeometryCopyBuilder.Type.CURVE
Curve or edge
|
static PartGeometryCopyBuilder.Type |
PartGeometryCopyBuilder.Type.CURVE_FEATURE
Curve-based feature
|
static PartGeometryCopyBuilder.Type |
PartGeometryCopyBuilder.Type.DATUM
Datum plane, datum axis or datum coordinate system feature
|
static PartGeometryCopyBuilder.Type |
PartGeometryCopyBuilder.Type.EXPRESSION
Expression
|
static PartGeometryCopyBuilder.Type |
PartGeometryCopyBuilder.Type.FACE
Face
|
static PartGeometryCopyBuilder.Type |
PartGeometryCopyBuilder.Type.PMI
PMI dimension
|
static PartGeometryCopyBuilder.Type |
PartGeometryCopyBuilder.Type.POINT
Point
|
static PartGeometryCopyBuilder.Type |
PartGeometryCopyBuilder.Type.ROUTING_OBJECT
Routing Object
|
static PartGeometryCopyBuilder.Type |
PartGeometryCopyBuilder.Type.SKETCH
Sketch feature
|
Modifier and Type | Method and Description |
---|---|
PartGeometryCopyBuilder.Type |
PartGeometryCopyBuilder.objectType()
Returns the type of object to be copied
License requirements: None. |
static PartGeometryCopyBuilder.Type |
PartGeometryCopyBuilder.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartGeometryCopyBuilder.Type |
PartGeometryCopyBuilder.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartGeometryCopyBuilder.Type[] |
PartGeometryCopyBuilder.Type.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
PartGeometryCopySelectBuilder |
PartGeometryCopyBuilder.createSelectionBuilder(PartGeometryCopyBuilder.Type objectType)
Creates a part geometry copy select builder
License requirements: None. |
void |
PartGeometryCopyBuilder.setObjectType(PartGeometryCopyBuilder.Type objectType)
License requirements: gateway ("UG GATEWAY") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.