Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static OffsetEdgeBuilder.OffsetEdgeMethod |
OffsetEdgeBuilder.OffsetEdgeMethod.ALONG_FACE |
static OffsetEdgeBuilder.OffsetEdgeMethod |
OffsetEdgeBuilder.OffsetEdgeMethod.ALONG_PLANEOF_EDGE |
Modifier and Type | Method and Description |
---|---|
OffsetEdgeBuilder.OffsetEdgeMethod |
OffsetEdgeBuilder.method()
Returns the method for offset edge
License requirements: None. |
static OffsetEdgeBuilder.OffsetEdgeMethod |
OffsetEdgeBuilder.OffsetEdgeMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OffsetEdgeBuilder.OffsetEdgeMethod |
OffsetEdgeBuilder.OffsetEdgeMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OffsetEdgeBuilder.OffsetEdgeMethod[] |
OffsetEdgeBuilder.OffsetEdgeMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OffsetEdgeBuilder.setMethod(OffsetEdgeBuilder.OffsetEdgeMethod method)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.