Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static OffsetEdgeBuilder.EndFaceBehaviourType |
OffsetEdgeBuilder.EndFaceBehaviourType.EXTEND |
static OffsetEdgeBuilder.EndFaceBehaviourType |
OffsetEdgeBuilder.EndFaceBehaviourType.MORPH |
Modifier and Type | Method and Description |
---|---|
OffsetEdgeBuilder.EndFaceBehaviourType |
OffsetEdgeBuilder.endFaceBehavior()
Returns whether fix side faces
License requirements: None. |
static OffsetEdgeBuilder.EndFaceBehaviourType |
OffsetEdgeBuilder.EndFaceBehaviourType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OffsetEdgeBuilder.EndFaceBehaviourType |
OffsetEdgeBuilder.EndFaceBehaviourType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OffsetEdgeBuilder.EndFaceBehaviourType[] |
OffsetEdgeBuilder.EndFaceBehaviourType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OffsetEdgeBuilder.setEndFaceBehavior(OffsetEdgeBuilder.EndFaceBehaviourType endFaceBehaviour)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.