Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static NSidedSurfaceBuilder.UVOrientationType |
NSidedSurfaceBuilder.UVOrientationType.AREA
area orientation
|
static NSidedSurfaceBuilder.UVOrientationType |
NSidedSurfaceBuilder.UVOrientationType.SPINE
spine orientation
|
static NSidedSurfaceBuilder.UVOrientationType |
NSidedSurfaceBuilder.UVOrientationType.VECTOR
vector orientation
|
Modifier and Type | Method and Description |
---|---|
NSidedSurfaceBuilder.UVOrientationType |
NSidedSurfaceBuilder.uvorientation()
Returns the UV orientation
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_1 ("basic freeform modeling") . |
static NSidedSurfaceBuilder.UVOrientationType |
NSidedSurfaceBuilder.UVOrientationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NSidedSurfaceBuilder.UVOrientationType |
NSidedSurfaceBuilder.UVOrientationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NSidedSurfaceBuilder.UVOrientationType[] |
NSidedSurfaceBuilder.UVOrientationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NSidedSurfaceBuilder.setUVOrientation(NSidedSurfaceBuilder.UVOrientationType button)
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_1 ("basic freeform modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.