Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static NSidedSurfaceBuilder.CenterControlType |
NSidedSurfaceBuilder.CenterControlType.POSITION
position type
|
static NSidedSurfaceBuilder.CenterControlType |
NSidedSurfaceBuilder.CenterControlType.TILTING
tilting type
|
Modifier and Type | Method and Description |
---|---|
static NSidedSurfaceBuilder.CenterControlType |
NSidedSurfaceBuilder.CenterControlType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NSidedSurfaceBuilder.CenterControlType |
NSidedSurfaceBuilder.CenterControlType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NSidedSurfaceBuilder.CenterControlType[] |
NSidedSurfaceBuilder.CenterControlType.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.