Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MoveEdgeBuilder.EndFaceBehaviorType |
MoveEdgeBuilder.EndFaceBehaviorType.EXTEND |
static MoveEdgeBuilder.EndFaceBehaviorType |
MoveEdgeBuilder.EndFaceBehaviorType.MORPH |
Modifier and Type | Method and Description |
---|---|
MoveEdgeBuilder.EndFaceBehaviorType |
MoveEdgeBuilder.endFaceBehavior()
Returns the end face setting.
|
static MoveEdgeBuilder.EndFaceBehaviorType |
MoveEdgeBuilder.EndFaceBehaviorType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MoveEdgeBuilder.EndFaceBehaviorType |
MoveEdgeBuilder.EndFaceBehaviorType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MoveEdgeBuilder.EndFaceBehaviorType[] |
MoveEdgeBuilder.EndFaceBehaviorType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MoveEdgeBuilder.setEndFaceBehavior(MoveEdgeBuilder.EndFaceBehaviorType type)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.