Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MirrorBodyBuilder.ParentPart |
MirrorBodyBuilder.ParentPart.OTHER_PART
Other Part
|
static MirrorBodyBuilder.ParentPart |
MirrorBodyBuilder.ParentPart.WORK_PART
Work Part
|
Modifier and Type | Method and Description |
---|---|
MirrorBodyBuilder.ParentPart |
MirrorBodyBuilder.parentPartType()
Returns the parent part type
License requirements: None. |
static MirrorBodyBuilder.ParentPart |
MirrorBodyBuilder.ParentPart.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorBodyBuilder.ParentPart |
MirrorBodyBuilder.ParentPart.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorBodyBuilder.ParentPart[] |
MirrorBodyBuilder.ParentPart.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MirrorBodyBuilder.setParentPartType(MirrorBodyBuilder.ParentPart sourceType)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.