Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MidSurfaceByFacePairsBuilder.PairingStrategyType |
MidSurfaceByFacePairsBuilder.PairingStrategyType.MANUAL
Manual pairing process
|
static MidSurfaceByFacePairsBuilder.PairingStrategyType |
MidSurfaceByFacePairsBuilder.PairingStrategyType.PROGRESSIVE
Progressive thickness is used
|
static MidSurfaceByFacePairsBuilder.PairingStrategyType |
MidSurfaceByFacePairsBuilder.PairingStrategyType.THICKNESS
Find all faces within search distance
|
Modifier and Type | Method and Description |
---|---|
MidSurfaceByFacePairsBuilder.PairingStrategyType |
MidSurfaceByFacePairsBuilder.pairingStrategy()
Returns the pairing strategy used by automatic pairs
License requirements: None. |
static MidSurfaceByFacePairsBuilder.PairingStrategyType |
MidSurfaceByFacePairsBuilder.PairingStrategyType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MidSurfaceByFacePairsBuilder.PairingStrategyType |
MidSurfaceByFacePairsBuilder.PairingStrategyType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MidSurfaceByFacePairsBuilder.PairingStrategyType[] |
MidSurfaceByFacePairsBuilder.PairingStrategyType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MidSurfaceByFacePairsBuilder.setPairingStrategy(MidSurfaceByFacePairsBuilder.PairingStrategyType pairingStrategy)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.