Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MatchEdgeBuilder.PoleMoveDirection |
MatchEdgeBuilder.PoleMoveDirection.X
Along XC direction
|
static MatchEdgeBuilder.PoleMoveDirection |
MatchEdgeBuilder.PoleMoveDirection.Y
Along YC direction
|
static MatchEdgeBuilder.PoleMoveDirection |
MatchEdgeBuilder.PoleMoveDirection.Z
Along ZC direction
|
Modifier and Type | Method and Description |
---|---|
MatchEdgeBuilder.PoleMoveDirection |
MatchEdgeBuilder.poleMoveDirectionEnum()
Returns the value indicating the direction of pole movement
License requirements: None. |
static MatchEdgeBuilder.PoleMoveDirection |
MatchEdgeBuilder.PoleMoveDirection.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MatchEdgeBuilder.PoleMoveDirection |
MatchEdgeBuilder.PoleMoveDirection.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MatchEdgeBuilder.PoleMoveDirection[] |
MatchEdgeBuilder.PoleMoveDirection.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MatchEdgeBuilder.setPoleMoveDirectionEnum(MatchEdgeBuilder.PoleMoveDirection poleMoveDirectionEnum)
License requirements: features_modeling ("FEATURES MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.