Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MatchEdgeBuilder.MatchExact |
MatchEdgeBuilder.MatchExact.ALIGN
Match align without change degree and patch
|
static MatchEdgeBuilder.MatchExact |
MatchEdgeBuilder.MatchExact.EXACT
Match exact
|
static MatchEdgeBuilder.MatchExact |
MatchEdgeBuilder.MatchExact.NONE
Don't match exact
|
Modifier and Type | Method and Description |
---|---|
MatchEdgeBuilder.MatchExact |
MatchEdgeBuilder.matchExactType()
Returns the value indicating type of exact match
License requirements: None. |
static MatchEdgeBuilder.MatchExact |
MatchEdgeBuilder.MatchExact.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MatchEdgeBuilder.MatchExact |
MatchEdgeBuilder.MatchExact.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MatchEdgeBuilder.MatchExact[] |
MatchEdgeBuilder.MatchExact.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MatchEdgeBuilder.setMatchExactType(MatchEdgeBuilder.MatchExact matchExact)
License requirements: features_modeling ("FEATURES MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.