Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MatchEdgeBuilder.EdgeConstraintType |
MatchEdgeBuilder.EdgeConstraintType.FREE
Free
|
static MatchEdgeBuilder.EdgeConstraintType |
MatchEdgeBuilder.EdgeConstraintType.ISO_U
Iso u
|
static MatchEdgeBuilder.EdgeConstraintType |
MatchEdgeBuilder.EdgeConstraintType.ISO_V
Iso v
|
static MatchEdgeBuilder.EdgeConstraintType |
MatchEdgeBuilder.EdgeConstraintType.LINEAR
Linear
|
static MatchEdgeBuilder.EdgeConstraintType |
MatchEdgeBuilder.EdgeConstraintType.LINKED
Linked, available for end edge only
|
static MatchEdgeBuilder.EdgeConstraintType |
MatchEdgeBuilder.EdgeConstraintType.PERPENDICULAR
Perpendicular
|
Modifier and Type | Method and Description |
---|---|
MatchEdgeBuilder.EdgeConstraintType |
MatchEdgeBuilder.endEdgeConstraint()
Returns the value indicating type of the end edge constraint
License requirements: None. |
MatchEdgeBuilder.EdgeConstraintType |
MatchEdgeBuilder.startEdgeConstraint()
Returns the value indicating type of the start edge constraint
License requirements: None. |
static MatchEdgeBuilder.EdgeConstraintType |
MatchEdgeBuilder.EdgeConstraintType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MatchEdgeBuilder.EdgeConstraintType |
MatchEdgeBuilder.EdgeConstraintType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MatchEdgeBuilder.EdgeConstraintType[] |
MatchEdgeBuilder.EdgeConstraintType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MatchEdgeBuilder.setEndEdgeConstraint(MatchEdgeBuilder.EdgeConstraintType endEdgeConstraint)
License requirements: features_modeling ("FEATURES MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
void |
MatchEdgeBuilder.setStartEdgeConstraint(MatchEdgeBuilder.EdgeConstraintType startEdgeConstraint)
License requirements: features_modeling ("FEATURES MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.