Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MapleBuilder.AssociativityEnum |
MapleBuilder.AssociativityEnum.EXISTING |
static MapleBuilder.AssociativityEnum |
MapleBuilder.AssociativityEnum.NEW |
static MapleBuilder.AssociativityEnum |
MapleBuilder.AssociativityEnum.NONE |
Modifier and Type | Method and Description |
---|---|
MapleBuilder.AssociativityEnum |
MapleBuilder.associativityEnumType()
Returns the associativity enum type
License requirements: None. |
static MapleBuilder.AssociativityEnum |
MapleBuilder.AssociativityEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MapleBuilder.AssociativityEnum |
MapleBuilder.AssociativityEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MapleBuilder.AssociativityEnum[] |
MapleBuilder.AssociativityEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MapleBuilder.setAssociativityEnumType(MapleBuilder.AssociativityEnum associativityEnumType)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.