Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static LawExtensionBuilderEx.Types |
LawExtensionBuilderEx.Types.FACES
Reference faces
|
static LawExtensionBuilderEx.Types |
LawExtensionBuilderEx.Types.VECTOR
Reference vector
|
Modifier and Type | Method and Description |
---|---|
LawExtensionBuilderEx.Types |
LawExtensionBuilderEx.type()
Returns the type
License requirements: None. |
static LawExtensionBuilderEx.Types |
LawExtensionBuilderEx.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LawExtensionBuilderEx.Types |
LawExtensionBuilderEx.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LawExtensionBuilderEx.Types[] |
LawExtensionBuilderEx.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LawExtensionBuilderEx.setType(LawExtensionBuilderEx.Types type)
License requirements: solid_modeling ("SOLIDS MODELING") OR free_form_modeling ("FREE-FORM MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.