Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static LawExtensionBuilderEx.OppositeSideExtensionOptions |
LawExtensionBuilderEx.OppositeSideExtensionOptions.ASYMMETRIC
Asymmetric extension
|
static LawExtensionBuilderEx.OppositeSideExtensionOptions |
LawExtensionBuilderEx.OppositeSideExtensionOptions.NONE
No extension
|
static LawExtensionBuilderEx.OppositeSideExtensionOptions |
LawExtensionBuilderEx.OppositeSideExtensionOptions.SYMMETRIC
Symmetric extension
|
Modifier and Type | Method and Description |
---|---|
LawExtensionBuilderEx.OppositeSideExtensionOptions |
LawExtensionBuilderEx.oppositeSideExtensionOption()
Returns the opposite side extension option
License requirements: None. |
static LawExtensionBuilderEx.OppositeSideExtensionOptions |
LawExtensionBuilderEx.OppositeSideExtensionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LawExtensionBuilderEx.OppositeSideExtensionOptions |
LawExtensionBuilderEx.OppositeSideExtensionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LawExtensionBuilderEx.OppositeSideExtensionOptions[] |
LawExtensionBuilderEx.OppositeSideExtensionOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LawExtensionBuilderEx.setOppositeSideExtensionOption(LawExtensionBuilderEx.OppositeSideExtensionOptions oppositeSideExtension)
License requirements: solid_modeling ("SOLIDS MODELING") OR free_form_modeling ("FREE-FORM MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.