Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static JoinCurvesBuilder.OutputCurve |
JoinCurvesBuilder.OutputCurve.ADVANCED
Advanced output curve
|
static JoinCurvesBuilder.OutputCurve |
JoinCurvesBuilder.OutputCurve.CUBIC
Cubic output curve
|
static JoinCurvesBuilder.OutputCurve |
JoinCurvesBuilder.OutputCurve.GENERAL
General output curve
|
static JoinCurvesBuilder.OutputCurve |
JoinCurvesBuilder.OutputCurve.QUINTIC
Quintic output curve
|
Modifier and Type | Method and Description |
---|---|
JoinCurvesBuilder.OutputCurve |
JoinCurvesBuilder.outputCurveType()
Returns the output curve type.
|
static JoinCurvesBuilder.OutputCurve |
JoinCurvesBuilder.OutputCurve.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static JoinCurvesBuilder.OutputCurve |
JoinCurvesBuilder.OutputCurve.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static JoinCurvesBuilder.OutputCurve[] |
JoinCurvesBuilder.OutputCurve.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
JoinCurvesBuilder.setOutputCurveType(JoinCurvesBuilder.OutputCurve outputCurveType)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.