Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static IsoparametricCurvesBuilder.DirectionTypes |
IsoparametricCurvesBuilder.DirectionTypes.ISO_U
Iso U direction
|
static IsoparametricCurvesBuilder.DirectionTypes |
IsoparametricCurvesBuilder.DirectionTypes.ISO_UV
Iso U and Iso V direction
|
static IsoparametricCurvesBuilder.DirectionTypes |
IsoparametricCurvesBuilder.DirectionTypes.ISO_V
Iso V direction
|
Modifier and Type | Method and Description |
---|---|
IsoparametricCurvesBuilder.DirectionTypes |
IsoparametricCurvesBuilder.direction()
Returns the direction type
License requirements: None. |
static IsoparametricCurvesBuilder.DirectionTypes |
IsoparametricCurvesBuilder.DirectionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static IsoparametricCurvesBuilder.DirectionTypes |
IsoparametricCurvesBuilder.DirectionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static IsoparametricCurvesBuilder.DirectionTypes[] |
IsoparametricCurvesBuilder.DirectionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
IsoparametricCurvesBuilder.setDirection(IsoparametricCurvesBuilder.DirectionTypes direction)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.