Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Interface and Description |
---|---|
interface |
AestheticFaceBlend
Represents an aesthetic face blend feature
To create or edit an instance of this class, use AestheticFaceBlendBuilder Created in NX7.5.0 |
interface |
FaceBlend
Represents a Face Blend feature.
|
interface |
SoftBlend
Represents a Soft Blend feature.
|
interface |
StyledBlend
Represents a styled blend feature
To create or edit an instance of this class, use StyledBlendBuilder Created in NX6.0.0 |
interface |
StyledCorner
Represents a styled corner feature
To create or edit an instance of this class, use StyledCornerBuilder Created in NX6.0.0 |
interface |
TrimAndExtend
Represents a trim and extend feature
To create or edit an instance of this class, use TrimAndExtendBuilder Created in NX9.0.0 |
interface |
TrimExtend
Represents a trim extend feature
To create or edit an instance of this class, use TrimExtendBuilder Created in NX5.0.0 |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.