Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static HolePackageBuilder.ThreadRotationOptions |
HolePackageBuilder.ThreadRotationOptions.LEFT
Left rotation
|
static HolePackageBuilder.ThreadRotationOptions |
HolePackageBuilder.ThreadRotationOptions.RIGHT
Right rotation
|
Modifier and Type | Method and Description |
---|---|
HolePackageBuilder.ThreadRotationOptions |
HolePackageBuilder.threadRotation()
Returns the thread rotation - this is applicable for threaded hole
License requirements: None. |
static HolePackageBuilder.ThreadRotationOptions |
HolePackageBuilder.ThreadRotationOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HolePackageBuilder.ThreadRotationOptions |
HolePackageBuilder.ThreadRotationOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HolePackageBuilder.ThreadRotationOptions[] |
HolePackageBuilder.ThreadRotationOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HolePackageBuilder.setThreadRotation(HolePackageBuilder.ThreadRotationOptions threadRotation)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.