Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static HolePackageBuilder.HoleForms |
HolePackageBuilder.HoleForms.COUNTERBORED
Counterbored hole form
|
static HolePackageBuilder.HoleForms |
HolePackageBuilder.HoleForms.COUNTERSINK
Countersink hole form
|
static HolePackageBuilder.HoleForms |
HolePackageBuilder.HoleForms.SIMPLE
Simple hole form
|
static HolePackageBuilder.HoleForms |
HolePackageBuilder.HoleForms.TAPERED
Tapered hole form
|
Modifier and Type | Method and Description |
---|---|
HolePackageBuilder.HoleForms |
HolePackageBuilder.generalHoleForm()
Returns the hole form - this is applicable for general hole
License requirements: None. |
HolePackageBuilder.HoleForms |
HolePackageBuilder.screwClearanceHoleForm()
Returns the hole form - this is applicable for screw clearance hole
License requirements: None. |
static HolePackageBuilder.HoleForms |
HolePackageBuilder.HoleForms.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HolePackageBuilder.HoleForms |
HolePackageBuilder.HoleForms.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HolePackageBuilder.HoleForms[] |
HolePackageBuilder.HoleForms.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HolePackageBuilder.setGeneralHoleForm(HolePackageBuilder.HoleForms holeForm)
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
HolePackageBuilder.setScrewClearanceHoleForm(HolePackageBuilder.HoleForms holeForm)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.