Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static HelixBuilder.OrientationOptions |
HelixBuilder.OrientationOptions.INFERRED
Local coordinate system is inferred from spine, at the start
|
static HelixBuilder.OrientationOptions |
HelixBuilder.OrientationOptions.SPECIFIED
Local coordinate system is specified by the user.
|
Modifier and Type | Method and Description |
---|---|
HelixBuilder.OrientationOptions |
HelixBuilder.orientationOption()
Returns the orientation option
License requirements: None. |
static HelixBuilder.OrientationOptions |
HelixBuilder.OrientationOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HelixBuilder.OrientationOptions |
HelixBuilder.OrientationOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HelixBuilder.OrientationOptions[] |
HelixBuilder.OrientationOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HelixBuilder.setOrientationOption(HelixBuilder.OrientationOptions orientationOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.