Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static GuidedExtensionBuilderEx.Types |
GuidedExtensionBuilderEx.Types.TANGENT_FROM_FACES
Extend tangentially from faces
|
static GuidedExtensionBuilderEx.Types |
GuidedExtensionBuilderEx.Types.VECTOR
Perpendicular to a vector
|
Modifier and Type | Method and Description |
---|---|
GuidedExtensionBuilderEx.Types |
GuidedExtensionBuilderEx.type()
Returns the option type to create guided extension surface
License requirements: solid_modeling ("SOLIDS MODELING") OR nx_freeform_2 ("advanced freeform modeling") OR ug_mold_design ("UG MOLD") OR die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
static GuidedExtensionBuilderEx.Types |
GuidedExtensionBuilderEx.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GuidedExtensionBuilderEx.Types |
GuidedExtensionBuilderEx.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GuidedExtensionBuilderEx.Types[] |
GuidedExtensionBuilderEx.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GuidedExtensionBuilderEx.setType(GuidedExtensionBuilderEx.Types type)
License requirements: solid_modeling ("SOLIDS MODELING") OR nx_freeform_2 ("advanced freeform modeling") OR ug_mold_design ("UG MOLD") OR die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.