Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Method and Description |
---|---|
GlobalShapingPointOffsetBuilder |
GlobalShapingPointOffsetBuilderList.findItem(int index)
Returns the object at the input index.
|
GlobalShapingPointOffsetBuilder[] |
GlobalShapingPointOffsetBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
GlobalShapingPointOffsetBuilder |
GlobalShapingBuilder.newTargetPoint()
Create a new target point
License requirements: solid_modeling ("SOLIDS MODELING") . |
Modifier and Type | Method and Description |
---|---|
void |
GlobalShapingPointOffsetBuilderList.append(GlobalShapingPointOffsetBuilder object)
Appends an object to the list
License requirements: None. |
void |
GlobalShapingPointOffsetBuilderList.append(GlobalShapingPointOffsetBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
GlobalShapingPointOffsetBuilderList.erase(GlobalShapingPointOffsetBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
GlobalShapingPointOffsetBuilderList.erase(GlobalShapingPointOffsetBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
GlobalShapingPointOffsetBuilderList.findIndex(GlobalShapingPointOffsetBuilder obj)
Finds the index where the input object appears.
|
void |
GlobalShapingPointOffsetBuilderList.insert(int location,
GlobalShapingPointOffsetBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
GlobalShapingPointOffsetBuilderList.setContents(GlobalShapingPointOffsetBuilder[] objects)
Sets the contents of the entire list.
|
void |
GlobalShapingPointOffsetBuilderList.swap(GlobalShapingPointOffsetBuilder object1,
GlobalShapingPointOffsetBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.