Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static GlobalShapingBuilder.RotationMethod |
GlobalShapingBuilder.RotationMethod.CONSTANT
Constant anlge rotation
|
static GlobalShapingBuilder.RotationMethod |
GlobalShapingBuilder.RotationMethod.CURVE_DEFINED
Curve interpolated rotation
|
static GlobalShapingBuilder.RotationMethod |
GlobalShapingBuilder.RotationMethod.LAW_CONTROLLED
Law controlled rotation
|
Modifier and Type | Method and Description |
---|---|
GlobalShapingBuilder.RotationMethod |
GlobalShapingBuilder.rotationAngleType()
Returns the rotation angle type
License requirements: None. |
static GlobalShapingBuilder.RotationMethod |
GlobalShapingBuilder.RotationMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GlobalShapingBuilder.RotationMethod |
GlobalShapingBuilder.RotationMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GlobalShapingBuilder.RotationMethod[] |
GlobalShapingBuilder.RotationMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GlobalShapingBuilder.setRotationAngleType(GlobalShapingBuilder.RotationMethod rotationAngleType)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.