Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static GlobalShapingBuilder.DirectionMethodType |
GlobalShapingBuilder.DirectionMethodType.NONE
Overcrown has no direction specified
|
static GlobalShapingBuilder.DirectionMethodType |
GlobalShapingBuilder.DirectionMethodType.NORMAL_TO_BASE
Overcrown is normal to base surface
|
static GlobalShapingBuilder.DirectionMethodType |
GlobalShapingBuilder.DirectionMethodType.NORMAL_TO_CONTROL
Overcrown is normal to control surface
|
static GlobalShapingBuilder.DirectionMethodType |
GlobalShapingBuilder.DirectionMethodType.NORMAL_TO_SHEET
Overcrown is normal to sheet
|
static GlobalShapingBuilder.DirectionMethodType |
GlobalShapingBuilder.DirectionMethodType.SAME_AS_PROJECTION
Overcrown is same as projection direction
|
static GlobalShapingBuilder.DirectionMethodType |
GlobalShapingBuilder.DirectionMethodType.SPECIFIED_DIRECTION
Overcrown is user specified direction
|
Modifier and Type | Method and Description |
---|---|
GlobalShapingBuilder.DirectionMethodType |
GlobalShapingBuilder.deformationDirectionMethod()
Returns the deformation direction method
License requirements: None. |
static GlobalShapingBuilder.DirectionMethodType |
GlobalShapingBuilder.DirectionMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GlobalShapingBuilder.DirectionMethodType |
GlobalShapingBuilder.DirectionMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GlobalShapingBuilder.DirectionMethodType[] |
GlobalShapingBuilder.DirectionMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GlobalShapingBuilder.setDeformationDirectionMethod(GlobalShapingBuilder.DirectionMethodType deformationDirectionMethod)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.