Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static GeometricConstraintData.AutoConstraintType |
GeometricConstraintData.AutoConstraintType.CURVATURE
Curvature(G2)
|
static GeometricConstraintData.AutoConstraintType |
GeometricConstraintData.AutoConstraintType.CURVATURE_DERIVATIVE
Curvature derivative(G3)
|
static GeometricConstraintData.AutoConstraintType |
GeometricConstraintData.AutoConstraintType.NONE
No automatic constraint
|
static GeometricConstraintData.AutoConstraintType |
GeometricConstraintData.AutoConstraintType.TANGENT
Tangent(G1)
|
Modifier and Type | Method and Description |
---|---|
GeometricConstraintData.AutoConstraintType |
GeometricConstraintData.automaticConstraintType()
Returns the automatic constraint type
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
static GeometricConstraintData.AutoConstraintType |
GeometricConstraintData.AutoConstraintType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeometricConstraintData.AutoConstraintType |
GeometricConstraintData.AutoConstraintType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeometricConstraintData.AutoConstraintType[] |
GeometricConstraintData.AutoConstraintType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GeometricConstraintData.setAutomaticConstraintType(GeometricConstraintData.AutoConstraintType autoConstraintType)
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.