Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static GeneralConicBuilder.Types |
GeneralConicBuilder.Types.COEFFICIENTS
Coefficient values and
GeneralConicBuilder.coefficientCSYS() and GeneralConicBuilder.setCoefficientCSYS(nxopen.CoordinateSystem) |
static GeneralConicBuilder.Types |
GeneralConicBuilder.Types.FIVE_POINTS
Five points, no slopes, no anchor, no rho value
|
static GeneralConicBuilder.Types |
GeneralConicBuilder.Types.FOUR_POINTS_ONE_SLOPE
Four points, one slope, no anchor, no rho value
|
static GeneralConicBuilder.Types |
GeneralConicBuilder.Types.THREE_POINTS_ANCHOR
Three points, no slopes, anchor, no rho value
|
static GeneralConicBuilder.Types |
GeneralConicBuilder.Types.THREE_POINTS_TWO_SLOPES
Three points, two slopes, no anchor, no rho value
|
static GeneralConicBuilder.Types |
GeneralConicBuilder.Types.TWO_POINTS_ANCHOR_RHO
Two points, no slopes, anchor, rho value
|
static GeneralConicBuilder.Types |
GeneralConicBuilder.Types.TWO_POINTS_TWO_SLOPES_RHO
Two points, two slopes, no anchor, rho value
|
Modifier and Type | Method and Description |
---|---|
GeneralConicBuilder.Types |
GeneralConicBuilder.type()
Returns the conic creation type.
|
static GeneralConicBuilder.Types |
GeneralConicBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeneralConicBuilder.Types |
GeneralConicBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeneralConicBuilder.Types[] |
GeneralConicBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GeneralConicBuilder.setType(GeneralConicBuilder.Types type)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.