Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static FitCurveBuilder.TargetSourceTypes |
FitCurveBuilder.TargetSourceTypes.CHAINED_POINTS
Chain using one or two points
|
static FitCurveBuilder.TargetSourceTypes |
FitCurveBuilder.TargetSourceTypes.CURVE
Curve
|
static FitCurveBuilder.TargetSourceTypes |
FitCurveBuilder.TargetSourceTypes.FACE
Face
|
static FitCurveBuilder.TargetSourceTypes |
FitCurveBuilder.TargetSourceTypes.FACET_BODY
Facet body
|
static FitCurveBuilder.TargetSourceTypes |
FitCurveBuilder.TargetSourceTypes.INFER
Infer target from selection
|
static FitCurveBuilder.TargetSourceTypes |
FitCurveBuilder.TargetSourceTypes.SPECIFIED_POINTS
Specified points
|
Modifier and Type | Method and Description |
---|---|
FitCurveBuilder.TargetSourceTypes |
FitCurveBuilder.targetSourceType()
Returns the target type
License requirements: None. |
static FitCurveBuilder.TargetSourceTypes |
FitCurveBuilder.TargetSourceTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FitCurveBuilder.TargetSourceTypes |
FitCurveBuilder.TargetSourceTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FitCurveBuilder.TargetSourceTypes[] |
FitCurveBuilder.TargetSourceTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FitCurveBuilder.setTargetSourceType(FitCurveBuilder.TargetSourceTypes targetSourceType)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.