Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static FillHoleBuilder.ShapeControlTypes |
FillHoleBuilder.ShapeControlTypes.FIT_TO_FACET |
static FillHoleBuilder.ShapeControlTypes |
FillHoleBuilder.ShapeControlTypes.FIT_TO_POINTS |
static FillHoleBuilder.ShapeControlTypes |
FillHoleBuilder.ShapeControlTypes.FULLNESS |
static FillHoleBuilder.ShapeControlTypes |
FillHoleBuilder.ShapeControlTypes.NONE |
static FillHoleBuilder.ShapeControlTypes |
FillHoleBuilder.ShapeControlTypes.PASS_THROUGH_CURVES |
Modifier and Type | Method and Description |
---|---|
FillHoleBuilder.ShapeControlTypes |
FillHoleBuilder.shapeControlType()
Returns the shape control type
License requirements: None. |
static FillHoleBuilder.ShapeControlTypes |
FillHoleBuilder.ShapeControlTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FillHoleBuilder.ShapeControlTypes |
FillHoleBuilder.ShapeControlTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FillHoleBuilder.ShapeControlTypes[] |
FillHoleBuilder.ShapeControlTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FillHoleBuilder.setShapeControlType(FillHoleBuilder.ShapeControlTypes shapeControlType)
License requirements: nx_freeform_1 ("basic freeform modeling"), solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.