Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static FaceBlendBuilder.RhoMethod |
FaceBlendBuilder.RhoMethod.ABSOLUTE
Absolute (NX) rho type
|
static FaceBlendBuilder.RhoMethod |
FaceBlendBuilder.RhoMethod.RELATIVE
Relative (I-deas) rho type
|
Modifier and Type | Method and Description |
---|---|
FaceBlendBuilder.RhoMethod |
FaceBlendBuilder.rhoType()
Returns the rho type for face blend
License requirements: None. |
static FaceBlendBuilder.RhoMethod |
FaceBlendBuilder.RhoMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FaceBlendBuilder.RhoMethod |
FaceBlendBuilder.RhoMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FaceBlendBuilder.RhoMethod[] |
FaceBlendBuilder.RhoMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FaceBlendBuilder.setRhoType(FaceBlendBuilder.RhoMethod rhoMethod)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.