Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static FaceBlendBuilder.OverflowMethod |
FaceBlendBuilder.OverflowMethod.NONE
No overflow option
|
static FaceBlendBuilder.OverflowMethod |
FaceBlendBuilder.OverflowMethod.NOTCH
Notch or Maintain Blend And Move Sharp Edges option
|
Modifier and Type | Method and Description |
---|---|
FaceBlendBuilder.OverflowMethod |
FaceBlendBuilder.overflowOption()
Returns the overflow option for face blend
License requirements: None. |
static FaceBlendBuilder.OverflowMethod |
FaceBlendBuilder.OverflowMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FaceBlendBuilder.OverflowMethod |
FaceBlendBuilder.OverflowMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FaceBlendBuilder.OverflowMethod[] |
FaceBlendBuilder.OverflowMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FaceBlendBuilder.setOverflowOption(FaceBlendBuilder.OverflowMethod option)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.