Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ExtractFaceBuilder.ParentPartType |
ExtractFaceBuilder.ParentPartType.OTHER_PART
inter part mode
|
static ExtractFaceBuilder.ParentPartType |
ExtractFaceBuilder.ParentPartType.POSITION_INDEPENDENT
position independent mode
|
static ExtractFaceBuilder.ParentPartType |
ExtractFaceBuilder.ParentPartType.WORK_PART
intra part mode
|
Modifier and Type | Method and Description |
---|---|
ExtractFaceBuilder.ParentPartType |
ExtractFaceBuilder.parentPart()
Returns the source part type
License requirements: None. |
static ExtractFaceBuilder.ParentPartType |
ExtractFaceBuilder.ParentPartType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExtractFaceBuilder.ParentPartType |
ExtractFaceBuilder.ParentPartType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExtractFaceBuilder.ParentPartType[] |
ExtractFaceBuilder.ParentPartType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ExtractFaceBuilder.setParentPart(ExtractFaceBuilder.ParentPartType parentPart)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.