Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ExtractFaceBuilder.FaceSurfaceType |
ExtractFaceBuilder.FaceSurfaceType.GENERAL_BSURFACE
extracted surface is a B-surface approximation of the original surface
|
static ExtractFaceBuilder.FaceSurfaceType |
ExtractFaceBuilder.FaceSurfaceType.POLYNOMIAL_CUBIC
extracted surface is a cubic polynomial approximation of the original surface
|
static ExtractFaceBuilder.FaceSurfaceType |
ExtractFaceBuilder.FaceSurfaceType.SAME_AS_ORIGINAL
extracted surface is the same as the original surface
|
Modifier and Type | Method and Description |
---|---|
ExtractFaceBuilder.FaceSurfaceType |
ExtractFaceBuilder.surfaceType()
Returns the surface type
License requirements: None. |
static ExtractFaceBuilder.FaceSurfaceType |
ExtractFaceBuilder.FaceSurfaceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExtractFaceBuilder.FaceSurfaceType |
ExtractFaceBuilder.FaceSurfaceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExtractFaceBuilder.FaceSurfaceType[] |
ExtractFaceBuilder.FaceSurfaceType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ExtractFaceBuilder.setSurfaceType(ExtractFaceBuilder.FaceSurfaceType surfaceType)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.