Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ExtractFaceBuilder.FaceOptionType |
ExtractFaceBuilder.FaceOptionType.ADJACENT_FACES
adjacent face type
|
static ExtractFaceBuilder.FaceOptionType |
ExtractFaceBuilder.FaceOptionType.ALL_BODY_FACES
all faces of body option
|
static ExtractFaceBuilder.FaceOptionType |
ExtractFaceBuilder.FaceOptionType.FACE_CHAIN
selection intent option
|
static ExtractFaceBuilder.FaceOptionType |
ExtractFaceBuilder.FaceOptionType.SINGLE_FACE
single face type
|
Modifier and Type | Method and Description |
---|---|
ExtractFaceBuilder.FaceOptionType |
ExtractFaceBuilder.faceOption()
Returns the face option type
License requirements: None. |
static ExtractFaceBuilder.FaceOptionType |
ExtractFaceBuilder.FaceOptionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExtractFaceBuilder.FaceOptionType |
ExtractFaceBuilder.FaceOptionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExtractFaceBuilder.FaceOptionType[] |
ExtractFaceBuilder.FaceOptionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ExtractFaceBuilder.setFaceOption(ExtractFaceBuilder.FaceOptionType faceOptionType)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.