Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ExtractFaceBuilder.ExtractType |
ExtractFaceBuilder.ExtractType.BODY
type to extract body
|
static ExtractFaceBuilder.ExtractType |
ExtractFaceBuilder.ExtractType.FACE
type to extract face
|
static ExtractFaceBuilder.ExtractType |
ExtractFaceBuilder.ExtractType.REGION_OF_FACES
type to extract region
|
Modifier and Type | Method and Description |
---|---|
ExtractFaceBuilder.ExtractType |
ExtractFaceBuilder.type()
Returns the type
License requirements: None. |
static ExtractFaceBuilder.ExtractType |
ExtractFaceBuilder.ExtractType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExtractFaceBuilder.ExtractType |
ExtractFaceBuilder.ExtractType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExtractFaceBuilder.ExtractType[] |
ExtractFaceBuilder.ExtractType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ExtractFaceBuilder.setType(ExtractFaceBuilder.ExtractType type)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.