Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static EmbossLimit.EndcapSourceOption |
EmbossLimit.EndcapSourceOption.FACE
Indicates the geometries are selected surfaces not on the target.
|
static EmbossLimit.EndcapSourceOption |
EmbossLimit.EndcapSourceOption.PLANE
Indicates the geometry is datum plane.
|
static EmbossLimit.EndcapSourceOption |
EmbossLimit.EndcapSourceOption.SECTION
Indicates the geometry is the sketch plane on which the section resides.
|
static EmbossLimit.EndcapSourceOption |
EmbossLimit.EndcapSourceOption.TARGET
Indicates the geometries are some of the faces on the Target Body.
|
Modifier and Type | Method and Description |
---|---|
EmbossLimit.EndcapSourceOption |
EmbossLimit.endcapSource()
Returns the endcap source option to decide where the End-Cap comes from
License requirements: None. |
static EmbossLimit.EndcapSourceOption |
EmbossLimit.EndcapSourceOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EmbossLimit.EndcapSourceOption |
EmbossLimit.EndcapSourceOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EmbossLimit.EndcapSourceOption[] |
EmbossLimit.EndcapSourceOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EmbossLimit.setEndcapSource(EmbossLimit.EndcapSourceOption endcapSourceOption)
Sets the endcap source option to decide where the End-Cap comes from
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.