Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static EmbossJoggle.JoggleDirectionMethod |
EmbossJoggle.JoggleDirectionMethod.NORMAL
Indicates joggle direction to along normal of target.
|
static EmbossJoggle.JoggleDirectionMethod |
EmbossJoggle.JoggleDirectionMethod.SIDEWALL
Indicates joggle direction to along sidewall direction.
|
static EmbossJoggle.JoggleDirectionMethod |
EmbossJoggle.JoggleDirectionMethod.SPECIFY
Indicates joggle direction to along user specified direction
|
Modifier and Type | Method and Description |
---|---|
EmbossJoggle.JoggleDirectionMethod |
EmbossJoggle.directionOption()
Returns the emboss joggle direction option
License requirements: None. |
static EmbossJoggle.JoggleDirectionMethod |
EmbossJoggle.JoggleDirectionMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EmbossJoggle.JoggleDirectionMethod |
EmbossJoggle.JoggleDirectionMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EmbossJoggle.JoggleDirectionMethod[] |
EmbossJoggle.JoggleDirectionMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EmbossJoggle.setDirectionOption(EmbossJoggle.JoggleDirectionMethod joggleOption)
Sets the emboss joggle direction option
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.