Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static EdgeSymmetryBuilder.MovementDirections |
EdgeSymmetryBuilder.MovementDirections.X
Along XC direction
|
static EdgeSymmetryBuilder.MovementDirections |
EdgeSymmetryBuilder.MovementDirections.Y
Along YC direction
|
static EdgeSymmetryBuilder.MovementDirections |
EdgeSymmetryBuilder.MovementDirections.Z
Along ZC direction
|
Modifier and Type | Method and Description |
---|---|
EdgeSymmetryBuilder.MovementDirections |
EdgeSymmetryBuilder.movementDirection()
Returns the value indicating the direction of pole movement during match
License requirements: None. |
static EdgeSymmetryBuilder.MovementDirections |
EdgeSymmetryBuilder.MovementDirections.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EdgeSymmetryBuilder.MovementDirections |
EdgeSymmetryBuilder.MovementDirections.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EdgeSymmetryBuilder.MovementDirections[] |
EdgeSymmetryBuilder.MovementDirections.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EdgeSymmetryBuilder.setMovementDirection(EdgeSymmetryBuilder.MovementDirections movementDirection)
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.