Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static EdgeBlendBuilder.Setback |
EdgeBlendBuilder.Setback.INCLUDE_WITH_CORNER
Include with corner
|
static EdgeBlendBuilder.Setback |
EdgeBlendBuilder.Setback.SEPARATE_FROM_CORNER
Separate from corner
|
Modifier and Type | Method and Description |
---|---|
EdgeBlendBuilder.Setback |
EdgeBlendBuilder.setbackOption()
Returns the setback option for edge blend
License requirements: None. |
static EdgeBlendBuilder.Setback |
EdgeBlendBuilder.Setback.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EdgeBlendBuilder.Setback |
EdgeBlendBuilder.Setback.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EdgeBlendBuilder.Setback[] |
EdgeBlendBuilder.Setback.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EdgeBlendBuilder.setSetbackOption(EdgeBlendBuilder.Setback setbackOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.