Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DraftBuilder.Method |
DraftBuilder.Method.ISOCLINE
Indicates use of isocline algorithm to create draft.
|
static DraftBuilder.Method |
DraftBuilder.Method.TRUE_DRAFT
Indicates use of true draft algorithm to create draft.
|
Modifier and Type | Method and Description |
---|---|
DraftBuilder.Method |
DraftBuilder.draftIsoclineOrTruedraft()
Returns the Draft method
License requirements: solid_modeling ("SOLIDS MODELING") . |
static DraftBuilder.Method |
DraftBuilder.Method.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DraftBuilder.Method |
DraftBuilder.Method.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DraftBuilder.Method[] |
DraftBuilder.Method.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DraftBuilder.setDraftIsoclineOrTruedraft(DraftBuilder.Method draftMethod)
Sets the Draft method
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.