Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DraftBodyBuilder.RepairingPartingEdgeOption |
DraftBodyBuilder.RepairingPartingEdgeOption.NONE
No repair parting edge option is specified
|
static DraftBodyBuilder.RepairingPartingEdgeOption |
DraftBodyBuilder.RepairingPartingEdgeOption.WITH_FILLET
Repair concave miter corners with fillet
|
static DraftBodyBuilder.RepairingPartingEdgeOption |
DraftBodyBuilder.RepairingPartingEdgeOption.WITH_LINE_AND_FILLET
Repair concave miter corners with both fillet and line
|
Modifier and Type | Method and Description |
---|---|
DraftBodyBuilder.RepairingPartingEdgeOption |
DraftBodyBuilder.repairPartingEdge()
Returns the repairing parting edge
License requirements: None. |
static DraftBodyBuilder.RepairingPartingEdgeOption |
DraftBodyBuilder.RepairingPartingEdgeOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DraftBodyBuilder.RepairingPartingEdgeOption |
DraftBodyBuilder.RepairingPartingEdgeOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DraftBodyBuilder.RepairingPartingEdgeOption[] |
DraftBodyBuilder.RepairingPartingEdgeOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DraftBodyBuilder.setRepairPartingEdge(DraftBodyBuilder.RepairingPartingEdgeOption repairingPartingEdges)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.