Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DivideCurveBuilder.InputArcLengthDirectionFlag |
DivideCurveBuilder.InputArcLengthDirectionFlag.END
Input Arc length from end
|
static DivideCurveBuilder.InputArcLengthDirectionFlag |
DivideCurveBuilder.InputArcLengthDirectionFlag.START
Input Arc length from start
|
Modifier and Type | Method and Description |
---|---|
DivideCurveBuilder.InputArcLengthDirectionFlag |
DivideCurveBuilder.directionFlag()
Returns the input arc length direction flag
License requirements: None. |
static DivideCurveBuilder.InputArcLengthDirectionFlag |
DivideCurveBuilder.InputArcLengthDirectionFlag.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DivideCurveBuilder.InputArcLengthDirectionFlag |
DivideCurveBuilder.InputArcLengthDirectionFlag.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DivideCurveBuilder.InputArcLengthDirectionFlag[] |
DivideCurveBuilder.InputArcLengthDirectionFlag.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DivideCurveBuilder.setDirectionFlag(DivideCurveBuilder.InputArcLengthDirectionFlag directionFlag)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.