Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DeleteFaceBuilder.SetbackOptions |
DeleteFaceBuilder.SetbackOptions.NEIGHBOR_BLEND
Cap by setback along the neighbor of the selected blend.
|
static DeleteFaceBuilder.SetbackOptions |
DeleteFaceBuilder.SetbackOptions.SELECTED_BLEND
Cap by setback along the selected blend.
|
Modifier and Type | Method and Description |
---|---|
DeleteFaceBuilder.SetbackOptions |
DeleteFaceBuilder.setback()
Returns the set back options.
|
static DeleteFaceBuilder.SetbackOptions |
DeleteFaceBuilder.SetbackOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DeleteFaceBuilder.SetbackOptions |
DeleteFaceBuilder.SetbackOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DeleteFaceBuilder.SetbackOptions[] |
DeleteFaceBuilder.SetbackOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DeleteFaceBuilder.setSetback(DeleteFaceBuilder.SetbackOptions setback)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.