Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DeleteFaceBuilder.CapOptionValues |
DeleteFaceBuilder.CapOptionValues.FACE_OR_PLANE
face or plane.
|
static DeleteFaceBuilder.CapOptionValues |
DeleteFaceBuilder.CapOptionValues.NEW_PLANE
new plane.
|
Modifier and Type | Method and Description |
---|---|
DeleteFaceBuilder.CapOptionValues |
DeleteFaceBuilder.capOption()
Returns the cap option.
|
static DeleteFaceBuilder.CapOptionValues |
DeleteFaceBuilder.CapOptionValues.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DeleteFaceBuilder.CapOptionValues |
DeleteFaceBuilder.CapOptionValues.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DeleteFaceBuilder.CapOptionValues[] |
DeleteFaceBuilder.CapOptionValues.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DeleteFaceBuilder.setCapOption(DeleteFaceBuilder.CapOptionValues capOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.